SFP connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SFP connection

2,793 Views
rashmikj
Contributor III

Hi,

Iam working on custom card based on LS1046a Processor. We have connected two identical SFP+ connection(XFI1 Retimer with SFP cage) to Lane 0 and Lane 1 SERDES1 Module . (RCW value = 0x1133)

We are using LS1046ardb Kit device tree for linux booting. We modified the fsl-ls1046a-rdb.dts by following

ethernet@f0000 { /* 10GEC1 */
fixed-link = <1 1 1000 0 0>;  
phy-connection-type = "xgmii";
};

and removed this 

aqr106_phy: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c45";
interrupts = <0 131 4>;
reg = <0x0>;
};

We also modified the fsl-ls1046a-rdb-sdk.dts file with

ethernet@8 {
compatible = "fsl,dpa-ethernet";
fsl,fman-mac = <&enet6>;
dma-coherent;
};

But linux is detecting fm1-mac10 as SFP+ connected to Lane0 of serdes module. I am able to ping to this.

There is no signal /frame on SFP+ connected to Lane1 of serdes module.

Both of SFP+ modules are similar to each other and similar to LS1046ARDB Kit.

Kindly Help.

0 Kudos
Reply
5 Replies

2,774 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> But linux is detecting fm1-mac10 as SFP+ connected to Lane0 of serdes module.

> I am able to ping to this.

How this could be considering that XFI.9 is on the lane 0?

XFI9.jpg

 

0 Kudos
Reply

2,771 Views
rashmikj
Contributor III

Sir,

Sorry I made a mistake.

> But linux is detecting fm1-mac10 as SFP+ connected to Lane0 of serdes module.

It is connected to Lane1 of serdes module. fm1-mac10 is okay

The other SFP+ is connected to lane0 of serdes module and it is not working. We are not able to see any signal/ frame on this SFP+ connector.

0 Kudos
Reply

2,762 Views
ufedor
NXP Employee
NXP Employee

Please use CodeWarrior QCVS SerDes Validation tool to check the lane 0 integrity.

0 Kudos
Reply

2,790 Views
ufedor
NXP Employee
NXP Employee

Please provide:

1) complete DTS

2) U-Boot and Linux booting logs

3) "ifconfig -a" log

0 Kudos
Reply

2,779 Views
rashmikj
Contributor III

Please find attached files.

0 Kudos
Reply