SD_IMP_CAL_RX and SD_IMP_CAL_TX current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD_IMP_CAL_RX and SD_IMP_CAL_TX current

1,570 次查看
toddreed
Contributor I

How much current flows through the 100 and 200 ohm resistors on SD_IMP_CAL_RX and SD_IMP_CAL_TX?

 

Thanks,
Todd

 

0 项奖励
回复
1 回复

1,564 次查看
Bulat
NXP Employee
NXP Employee

You forgot to mention processor's name. Values 100 and 200 ohm point to e.g. a P2020 like device. Maximum theoretical current can be calculated as XVDD / 100 Ohm = 10mA for 100 Ohm resistor and XVDD / 200 Ohm = 5mA for 200 Ohm resistor.

Regards,

Bulat

 

0 项奖励
回复