Root file system is not mounted

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Root file system is not mounted

1,388件の閲覧回数
leelambjae
Contributor I

Hi 

We asked about root file system mount again.

We changed our bootm parameter but it didn't work yet.

We attach the image name what we use, boot script, and console window screen shot.

1.png

This is name of each image we use.

2.png

This is bootscript.

We make this bootscript using mkimage.

command is as follows:

~./mkimage -A ppc -T script -a 0 -e 0x40 -d bootscript.txt bootscript

3.png

This is the console window what we get.

We can't mount root file system yet.

Could you tell us how to do it??

Second question is secure u-boot patch.

Secure booting and normal booting use the same file system. And normal booting works well, but secure booting didn't work. So we think that secure u-boot has problem. (Is this right?)

When we change secure u-boot, do we have to change secure u-boot based on sdk u-boot source code? Or can secure u-boot changed based on u-boot of DENX?

ラベル(1)
0 件の賞賛
返信
1 返信

1,286件の閲覧回数
Pavel
NXP Employee
NXP Employee

It looks like that your "bootm" command contains incorrect address for root file system.

Test your script if manually set commands from this script.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信