Reg. TDM Clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg. TDM Clock

2,043件の閲覧回数
ibram
Contributor I

Hi,

we are using 2 TDM ports in P1021 based design. we have 2 doubts in using the clocks available in TDM interface.

1. As of now, we have a single clock sourcing both the TDMx_TXCLK and TDMx_RXCLCK and one more clock sourcing both TDMx_TSYNC and TDMx_RSYNC. Is there any way to configure a single pin for TDMx_TXCLK and TDMx_RXCLCK functions and the same for TDMx_TSYNC and TDMx_RSYNC functions?

2. Can we share one TDM CLOCK/SYNC to another TDM CLOCK/SYNC functions?

Please let me know if you need further explanation?

Regards,

Ibram

0 件の賞賛
返信
1 返信

1,690件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

1. Yes, please look SI mode register, "CRTx" field.

2. Yes, this configuration is possible.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信