Recommended SPI and Parallel Flash for T1040

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Recommended SPI and Parallel Flash for T1040

2,276 次查看
xarowubas
Contributor III

Hello,

Is there any recommended list of SPI and Parallel Flashes which can be interfaced with T1040 or the SOC is compatible with flashes by any manufacturer ? 

Thanks,

Xaro

标记 (3)
0 项奖励
回复
1 回复

2,159 次查看
ufedor
NXP Employee
NXP Employee

There is no such list because T1040 has universal controllers: IFC (for parallel NOR Flash) and eSPI (for SPI Flash).

The IFC features a NOR flash controller, which:
• Compatible with asynchronous NOR flash (synchronous burst-read not supported)
• Provides memory-mapped interfacing to NOR
• Supports an address data multiplexed (ADM) NOR device
• Flexible timing control allows interfacing with proprietary NOR devices (WE_B controlled writes only)
• Boot chip-select (CS0) is available at system reset
• Data bus width of 16-bits

The major features of the eSPI controller are:
• Interface contains SPI_MOSI, SPI_MISO, SPI_CLK, and 4 chip selects
• Supports eSPI master
• Supports RapidSTM full clock cycle operation
• Full-duplex or half-duplex master operation
• Supports Winbond dual output read
• Command in transaction level-easier for accessing eSPI devices
• Works with a range from 4-bit to 16-bit data characters
• Supports back-to-back character transmission and reception
• Supports reverse data mode for 8/16 bits data characters
• Supports single-master environment
• Maximum clock rate possible is (platform clock rate/ )
• Independent programmable baud rate generator
• Programmable clock phase and polarity.
• Supports four different configurations per chip select
• Local loopback capability for testing

0 项奖励
回复