Re: RAM Boot Using TFTP deployment on P4080-come-ds machine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: RAM Boot Using TFTP deployment on P4080-come-ds machine

1,960 Views
vishallinux
Contributor I

Dear Helper,

i am using p4080 board and just want to use Ram boot using TFTP.
using  Default-
 1) uboot.bin
 2) uImage-git-r2-p4080ds-20120827101516.bin - @1000000

3) uImage-git-r2-p4080ds-20120827101516.dtb - @c00000
4) fsl-image-minimal-p4080ds-20120827104008.rootfs.ext2.gz.u-boot @2000000
and after command -
 bootm 1000000 2000000 c00000

It is going to Stuck.......with this message--




fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 0.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 0 ports detected
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 45, io mem 0xffe211000
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mpc-i2c ffe118100.i2c: timeout 1000000 us
usb 2-1: new high speed USB device number 2 using fsl-ehci
hub 2-1:1.0: USB hub found
hub 2-1:1.0: 4 ports detected

Thanks & Regards'
Vishal Gupta
0 Kudos
Reply
1 Reply

1,631 Views
mattsm
Contributor III

Did you try the default images or are these one's you built yourself?

-M

0 Kudos
Reply