Ramdisk message

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ramdisk message

2,972件の閲覧回数
leelambjae
Fresh Out Contributor

DEAR ALL:

Hi 

We are trying to secure boot using T2080RDB-PC.

But it still didn't work. 

We have trouble in file system mount. 

I attached two pictures. 

KakaoTalk_20180911_125324655.jpg

KakaoTalk_20180911_125328654.jpg

First is normal boot log and second is secure boot .

There are "Loading Ramdisk to 2f8fd000, end 2ffff6ff ..OK" in the normal boot, but there are no message about ramdisk in secure boot log. 

Could you let us know the reason we can't mount file system ?? 

Is it related to message that"Loading Ramdisk ~~~" ? 

THANK YOU 

HAVE A GOOD DAY!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,789件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello yangjae lee,

In Secure boot, you need to deploy your rootfs filesystem at 0xE9300000 and the size should less than 29696K.

In secure boot bootscript, you need to use 0xE9300000 in the bootm command, and boot rootfs from NOR flash directly.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信