QorIQ for object caching solutions such as memcached

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ for object caching solutions such as memcached

1,222 Views
vakulgarg
NXP Employee
NXP Employee

I want to prototype a memcached solution based on some QorIQ processor.

What should be the selection criterion for the processor?

What kind of benchmarks are available for memcached?

Any info or help is appreciated.

Thanks

0 Kudos
Reply
2 Replies

1,101 Views
Pavel
NXP Employee
NXP Employee

Look at please AN2663 Cache promer (http://cache.freescale.com/files/32bit/doc/app_note/AN2663.pdf).

See please the AN2354 application note (http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2354.pdf)
See also benchmark results for the QorIQ processors on the following page: www.eembc.com.
0 Kudos
Reply

1,101 Views
bharatbhushan
NXP Employee
NXP Employee

Thanks for sharing the Application notes. These are core cache benchmarks and we are looking for object caching benchmarks with memchached solution.

Memcached is a object caching solution used in Data Center and some known benchmarks are memslap and brutis.

0 Kudos
Reply