QorIQ devices support on kernel mainline

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ devices support on kernel mainline

ソリューションへジャンプ
1,916件の閲覧回数
tiagobrusamarel
Contributor V

Hello,

Does kernel mainline fully support QorIQ devices yet?

0 件の賞賛
返信
1 解決策
1,791件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Section 2.1 of NXP SDK 2.0-1703 documentation:

The SDK is based upon the standard Linux kernel from http://www.kernel.org, but with patches added by the Yocto Project, NXP, and other community members to support NXP SoCs. Much of the NXP-supplied Linux software is within the kernel;

NXP is one of the top 20 global kernel.org contributors.

One or more times per year NXP will upgrade to the latest long-term supported kernel version; then throughout the year, the team will accumulate changes for that kernel version. Occasionally, NXP will produce an “off cycle” SDK release that adds specific support for a new IC using patches. NXP is experienced with porting code to the latest kernels, across several product lines and architectures, when it is needed by our customer base.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,792件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Section 2.1 of NXP SDK 2.0-1703 documentation:

The SDK is based upon the standard Linux kernel from http://www.kernel.org, but with patches added by the Yocto Project, NXP, and other community members to support NXP SoCs. Much of the NXP-supplied Linux software is within the kernel;

NXP is one of the top 20 global kernel.org contributors.

One or more times per year NXP will upgrade to the latest long-term supported kernel version; then throughout the year, the team will accumulate changes for that kernel version. Occasionally, NXP will produce an “off cycle” SDK release that adds specific support for a new IC using patches. NXP is experienced with porting code to the latest kernels, across several product lines and architectures, when it is needed by our customer base.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------