QorIQ Processor DDR Read/Write Margin Test availability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QorIQ Processor DDR Read/Write Margin Test availability

3,375件の閲覧回数
partharoy
Contributor II

Hello Support,

Within the QCVS DDR Validation User Guide, I find a statement that read/write margin test feature is not supported in all QorIQ Processor variants.

Can you please tell me in which variants of QorIQ processor, QCVS Read/Write margin test is unavailable?

Thank you.

Regards

Pashan

タグ(1)
0 件の賞賛
返信
4 返答(返信)

3,221件の閲覧回数
addiyi
NXP Employee
NXP Employee

You are interested in ARM or PA processors? For ARM based processors only for LS1012A/LS1024/LS102MA the read/write margin tests are not available.

Adrian

0 件の賞賛
返信

3,221件の閲覧回数
partharoy
Contributor II

Hello Adrian,

Thank you for the info regarding ARM based QorIQ.

For the PA Processors, read/write margin test are not available in which versions?

Regards

Pashan

0 件の賞賛
返信

3,221件の閲覧回数
addiyi
NXP Employee
NXP Employee

For PA you need to install QCVS 4.5 on top of CodeWarrior for PA 10.5.1.

Adrian

0 件の賞賛
返信

3,221件の閲覧回数
partharoy
Contributor II

Hello Adrian,

For the
PA processors, which parts doesn't support read/write margin test?

Thank you.

Regards

Partha

0 件の賞賛
返信