QorIQ Processor DDR Read/Write Margin Test availability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ Processor DDR Read/Write Margin Test availability

3,379 Views
partharoy
Contributor II

Hello Support,

Within the QCVS DDR Validation User Guide, I find a statement that read/write margin test feature is not supported in all QorIQ Processor variants.

Can you please tell me in which variants of QorIQ processor, QCVS Read/Write margin test is unavailable?

Thank you.

Regards

Pashan

Tags (1)
0 Kudos
Reply
4 Replies

3,225 Views
addiyi
NXP Employee
NXP Employee

You are interested in ARM or PA processors? For ARM based processors only for LS1012A/LS1024/LS102MA the read/write margin tests are not available.

Adrian

0 Kudos
Reply

3,225 Views
partharoy
Contributor II

Hello Adrian,

Thank you for the info regarding ARM based QorIQ.

For the PA Processors, read/write margin test are not available in which versions?

Regards

Pashan

0 Kudos
Reply

3,225 Views
addiyi
NXP Employee
NXP Employee

For PA you need to install QCVS 4.5 on top of CodeWarrior for PA 10.5.1.

Adrian

0 Kudos
Reply

3,225 Views
partharoy
Contributor II

Hello Adrian,

For the
PA processors, which parts doesn't support read/write margin test?

Thank you.

Regards

Partha

0 Kudos
Reply