QorIQ B4860 GPU and Refernce Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ B4860 GPU and Refernce Design

Jump to solution
2,590 Views
A-R
Contributor II

Hi,

I have two questions about QorIQ B4860 processor.

1) I want to run Ubuntu/ Windows on QorIQ B4860 processor. So is there any GPU available in this processor so that I can boot GUI based OS and can run some multimedia application on this processor.

2) I was looking for a board with QorIQ B4860 processor and I found QorIQ B4860BDS board with this processor. But I can't find any schematic and Board layout for this board. Is there any schematic and board layout available for this board? If yes how can I get those files?

0 Kudos
Reply
1 Solution
2,583 Views
ufedor
NXP Employee
NXP Employee

1) B4860 does not possess GPU.

2) Schematics is confidential and can be provided only under NDA.

NDA signing can be arranged by creating a Technical Case using corporate email:

https://support.nxp.com/s/

View solution in original post

0 Kudos
Reply
4 Replies
2,578 Views
A-R
Contributor II

Thanks for your reply. 

0 Kudos
Reply
2,584 Views
ufedor
NXP Employee
NXP Employee

1) B4860 does not possess GPU.

2) Schematics is confidential and can be provided only under NDA.

NDA signing can be arranged by creating a Technical Case using corporate email:

https://support.nxp.com/s/

0 Kudos
Reply
2,566 Views
A-R
Contributor II

One more thing. There is a reference design for B4860BDS at this link

It is written in above link that this reference design is NOT RECOMMENDED FOR NEW DESIGNS.

Can you tell me which reference design should i use for new design?

 

Tags (1)
0 Kudos
Reply
2,557 Views
ufedor
NXP Employee
NXP Employee

There is no new design for the B4860 - please refer to the information provided by the following link:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture/qoriq-communication-...

0 Kudos
Reply