QMan initialization problem in DPAA Normal Mode Implementation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QMan initialization problem in DPAA Normal Mode Implementation

1,264 次查看
coskunayyildiz
Contributor I

Dear ALL,

I am trying to implement DPAA Normal mode for our custom electronic

card, having P2041 processor on it. I have the following issue while

initializing QMan.

When I send one command to QMan (ex: Schedule, Query, Alter, vs.), it returns me that the command is successfuly performed. However, when I send another command to QMan, it does not return me anything. In order to be able to use DPAA, I have to send commands to QMan all the time so, I cannot use QMan properly now.

This is an urgent issue for us, I will appreciate any efforts that can lead me to solution.

Thanks in advance.

标记 (3)
0 项奖励
回复
0 回复数