QMan initialization problem in DPAA Normal Mode Implementation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QMan initialization problem in DPAA Normal Mode Implementation

1,242件の閲覧回数
coskunayyildiz
Contributor I

Dear ALL,

I am trying to implement DPAA Normal mode for our custom electronic

card, having P2041 processor on it. I have the following issue while

initializing QMan.

When I send one command to QMan (ex: Schedule, Query, Alter, vs.), it returns me that the command is successfuly performed. However, when I send another command to QMan, it does not return me anything. In order to be able to use DPAA, I have to send commands to QMan all the time so, I cannot use QMan properly now.

This is an urgent issue for us, I will appreciate any efforts that can lead me to solution.

Thanks in advance.

タグ(3)
0 件の賞賛
返信
0 返答(返信)