QCVS DDR tool Dozing State Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QCVS DDR tool Dozing State Error

2,296件の閲覧回数
efecanbozulu
Contributor I

Hello, we are trying to work our DDR4 discreet memory on a t1024 based custom board, the board is geting the RCW from SD card. We are using CW 10.5.1 for linux and using QCVS tool to obtain reasonable auto leveling values. However, we are not able to get any stable configuration from the tool. Under this case we had checked our procedure with t1023RDB, which also has the same discreet DDR4 memory on board. The tool is generating results for t1023RDB with the same condition (where the RCW is taken from SD card, only RCW no PBL data part or u-boot on SD card).

On QCVS DDR tool we are observing some strange configurations saying (In Red Boxes):

Core interrupted by exception: The tst was not executed, as the core was expected to be in Running state and instead it is in Dozing.

Which is indicating the the CPU is in doze state. Even though we are not doing anything with power management.

Results can be seen as:

pastedImage_3.png

Orange configurations are giving ACE errors. This might be an expected behaviour, however, we had tried to investigate the error of the red boxes and, we did not see anything related to this error in DDR tool of QCVS in any documentation or forum questions.

Can you help us about this issue?

タグ(5)
0 件の賞賛
返信
2 返答(返信)

1,838件の閲覧回数
Jaygao
Contributor I

have you resolved this problem?

0 件の賞賛
返信

2,133件の閲覧回数
ufedor
NXP Employee
NXP Employee

A red cell indicates that validation failed for the cell due to target connection issue.

Please doublecheck the JTAG interface connection circuit - refer to the AN4971 -  QorIQ T1024 Family Design Checklist, Figure 23. JTAG interface connection.

0 件の賞賛
返信