Programm the kernel and ramdisk into flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Programm the kernel and ramdisk into flash

1,827 次查看
valentinmovsik
Contributor I

Hi everyone,

I'm trying  to programm the kernel and ramdisk into flash with new img files and I need to supply to U-boot the next information :

1. <kernel_start_addr>

2. <ramdisk_start_addr>

3. <dtb_start_addr>

But I'm a little bit confuse. Where can I get the information ? From NOR Flash Memory Map Table ? Is the kernel_start_addr is equal to "Linux.uImage" ?

 

Thanks,

 

Val

0 项奖励
回复
2 回复数

1,690 次查看
Pavel
NXP Employee
NXP Employee

Yes, the . <kernel_start_addr>,  <ramdisk_start_addr> and  <dtb_start_addr> are available in "NOR Flash Memory Map".

These addresses are available for all board in SDK documentation. For example see the SDK 2.0 documentation:

http://www.nxp.com/files/soft_dev_tools/doc/support_info/QORIQ-SDK-2.0-IC-REV0.zip?fasp=1&WT_TYPE=Su...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,690 次查看
valentinmovsik
Contributor I

Hi Pavel,

Thank you for your response.

I've already found the correct information by myself. BTW I've had the document which you mentioned before, but the problem of this document for exmple in NOR Flash Memory Map they are talking about "Rootfs" and in the CLI command about "ramdisk_start_add". The explanation isn't clear enough.

Regards,

Val

0 项奖励
回复