Programm the kernel and ramdisk into flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programm the kernel and ramdisk into flash

1,828件の閲覧回数
valentinmovsik
Contributor I

Hi everyone,

I'm trying  to programm the kernel and ramdisk into flash with new img files and I need to supply to U-boot the next information :

1. <kernel_start_addr>

2. <ramdisk_start_addr>

3. <dtb_start_addr>

But I'm a little bit confuse. Where can I get the information ? From NOR Flash Memory Map Table ? Is the kernel_start_addr is equal to "Linux.uImage" ?

 

Thanks,

 

Val

0 件の賞賛
返信
2 返答(返信)

1,691件の閲覧回数
Pavel
NXP Employee
NXP Employee

Yes, the . <kernel_start_addr>,  <ramdisk_start_addr> and  <dtb_start_addr> are available in "NOR Flash Memory Map".

These addresses are available for all board in SDK documentation. For example see the SDK 2.0 documentation:

http://www.nxp.com/files/soft_dev_tools/doc/support_info/QORIQ-SDK-2.0-IC-REV0.zip?fasp=1&WT_TYPE=Su...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,691件の閲覧回数
valentinmovsik
Contributor I

Hi Pavel,

Thank you for your response.

I've already found the correct information by myself. BTW I've had the document which you mentioned before, but the problem of this document for exmple in NOR Flash Memory Map they are talking about "Rootfs" and in the CLI command about "ramdisk_start_add". The explanation isn't clear enough.

Regards,

Val

0 件の賞賛
返信