Product Inquiry

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Product Inquiry

1,386件の閲覧回数
hyun-pilkim
Contributor I

Is there a follow-up product of the P4080 PCIE adapter that supports 20 Gbps or higher?

(I want NIC development board like P4080PCIE)

If so,

Does the board support the latest Ubuntu or CentOS?

Does the board provide a sdk that allows programming to control the pcie and Ethernet links?

ラベル(1)
0 件の賞賛
返信
1 返信

1,255件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please consider T2080RDB:

QorIQ T2080 Reference Design Board|NXP 

> Does the board support the latest Ubuntu or CentOS

Third-party Operation Systems are not supported directly by NXP - please address the request to the OS developer.

> Does the board provide a sdk that allows programming to control the pcie and Ethernet links

Yes, Linux SDK is provided by NXP.

0 件の賞賛
返信