Problems compiling my linux kernel with bitbake

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problems compiling my linux kernel with bitbake

跳至解决方案
3,380 次查看
andreasschmelte
Contributor I

Hi,

I have a problem when I try to build my own kernel images for the twr-LS1021. I tried it with the virtual box and by installing the sdk on a native system (Ubuntu 14.04 32 Bit). I tried to setup my development system by downloading the sdk images (v1.7 and v2.0) and also by installing it as shown in the following link.

4. Create SDK — TWR-LS1021A A documentation

When I try to build my kernel, with hob or from the command line, I get the following error. In the command line I tried the commands "bitbake fsl-image-core" and "bitbake virtual/kernel". It is always the same error.

(The following messages are written in my log file, which is created automatically)

Head of the log file:

----------------------------------------------------------------------------

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "Ubuntu-14.04"

TARGET_SYS        = "arm-fsl-linux-gnueabi"

MACHINE           = "ls1021atwr"

DISTRO            = "fsl-networking"

DISTRO_VERSION    = "QorIQ-SDK-V1.8"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa7"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto       

meta-yocto-bsp    = "(nobranch):18837ea4cdd4fdab608e0a032a11a2dfb6b1ee1a"

meta-fsl-arm      = "(nobranch):b529ac5ba06a0d69d7e6e295776a4d684c6e1c56"

meta-fsl-networking = "(nobranch):6eb28ed659bbadfa470237dfce98bcbf53c18fe1"

meta-fsl-toolchain = "(nobranch):a253b3594d8d9e0a4ed869d1fb502c395c4438ac"

meta-virtualization = "(nobranch):df44ec7a68c8e4b713a458a5b93e903103dea85c"

meta-oe          

meta-networking  

meta-perl        

toolchain-layer   = "(nobranch):4a44c4107899363b22c01eb5621b0c86db1c659c"

meta-java         = "(nobranch):65c89b93fa9d4c89e1dfb5b795075cbadb541009"

meta-linaro-toolchain = "(nobranch):9e742fbb8cbb6d2087fb41429a77fcf0ce50dbb8"

meta-security     = "(nobranch):9f4c3849521465b459845dcc1a7a885bacaae9d9"

----------------------------------- Error message (section of the log) -----------------------------------------

WARNING: Failed to fetch URL git://git.freescale.com/ppc/sdk/asf.git;branch=master, attempting MIRRORS if available

ERROR: Fetcher failure: Unable to find revision 62ba10ab6bab8f8f53934e4bb55b5a552bf3fd6b in branch master even from upstream

ERROR: Function failed: Fetcher failure for URL: 'git://git.freescale.com/ppc/sdk/asf.git;branch=master'. Unable to fetch URL from any source.

NOTE: recipe asf-git-r0: task do_fetch: Failed

ERROR: Task 1589 (/home/architech/architech_sdk/architech/ls1021atwr/yocto/meta-fsl-arm/recipes-kernel/asf/asf_git.bb, do_fetch) failed with exit code '1'

NOTE: Running task 2049 of 3909 (ID: 981, /home/architech/architech_sdk/architech/ls1021atwr/yocto/poky/meta/recipes-extended/sysklogd/sysklogd_1.5.bb, do_configure)

NOTE: recipe sysklogd-1.5-r7: task do_configure: Succeeded

NOTE: recipe pkgconfig-0.28-r0: task do_configure: Succeeded

NOTE: recipe openssh-6.5p1-r0: task do_configure: Succeeded

NOTE: recipe linux-ls1-3.12-r0: task do_fetch: Succeeded

NOTE: Tasks Summary: Attempted 2049 tasks of which 15 didn't need to be rerun and 1 failed.

The failure happens independent from the environment where my system is running. In one environment I hav to use a proxy, the other network works without a proxy.

Can anyone explain me what the reason for this problem is?

Thanks for your help and kind regards,

Andreas Schmelter

0 项奖励
回复
1 解答
2,928 次查看
Pavel
NXP Employee
NXP Employee

Check your command sequence for this SDK using.

We usually use the following command sequence for SDK installing under Ubuntu 14.04 and Ubuntu 16.04:

  1. 1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos

  1. 2.  a) command: ls -l /bin/sh

                Message:  /bin/sh -> dash

    b) command: sudo dpkg-reconfigure dash

                Answer after password – No

                Message:

                Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

                Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

                Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

                Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

    c) command for checking: ls -l /bin/sh

                Message: /bin/sh -> bash

  1. 3. install SDK cache for QorIQ Linux SDK v2.0 CORTEXA7 Yocto Cache.iso
  2. 4. install SDK source
  3. 5. cd <sdk-install-dir>.
  4. 6. ./sources/meta-freescale/scripts/host-prepare.sh

Usually Linux recommends also run the following command: sudo usr/sbin/visudo

  1. 7. bitbake fsl-image-minimal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,928 次查看
andreasschmelte
Contributor I

Thank you!

The compilation of the kernel was successful.

Kind Regards

0 项奖励
回复
2,929 次查看
Pavel
NXP Employee
NXP Employee

Check your command sequence for this SDK using.

We usually use the following command sequence for SDK installing under Ubuntu 14.04 and Ubuntu 16.04:

  1. 1. sudo apt-get install ubuntu-minimal ubuntu-standard patch vim-common sed wget subversion git-core coreutils libbonobo2-common unzip texi2html texinfo libsdl1.2-dev docbook-utils gawk python-pysqlite2 diffstat make gcc build-essential xz-utils g++ desktop-file-utils chrpath libgl1-mesa-dev libglu1-mesa-dev autoconf automake groff libtool xterm libncurses5-dev cvs tofrodos

  1. 2.  a) command: ls -l /bin/sh

                Message:  /bin/sh -> dash

    b) command: sudo dpkg-reconfigure dash

                Answer after password – No

                Message:

                Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'

                Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'

                Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'

                Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'

    c) command for checking: ls -l /bin/sh

                Message: /bin/sh -> bash

  1. 3. install SDK cache for QorIQ Linux SDK v2.0 CORTEXA7 Yocto Cache.iso
  2. 4. install SDK source
  3. 5. cd <sdk-install-dir>.
  4. 6. ./sources/meta-freescale/scripts/host-prepare.sh

Usually Linux recommends also run the following command: sudo usr/sbin/visudo

  1. 7. bitbake fsl-image-minimal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------