Problem during setting own process Entry Address for U - Boot application.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem during setting own process Entry Address for U - Boot application.

1,555 Views
mvicki93
Contributor I

SUBJECT : How to Set my Own Process Entry Address for U-Boot Application?

We purchased an T4240 EVM Kit for developing, i compiled U-boot application on using below commands.

when we tried to assign our own process entry address, the compiler throws an warning :

#powerpc64-fsl-linux-ld flash.o -o app.o -Ttext=0x01000000

(warning : powerpc64-fsl-linux-ld: warning: cannot find entry symbol _start; defaulting to 0000000001010190 )

Step 1 : powerpc64-fsl-linux-gcc -c flash.c

Step 2 : powerpc64-fsl-linux-ld flash.o -o app.o -Ttext=0x01000000.

(warning : powerpc64-fsl-linux-ld: warning: cannot find entry symbol _start; defaulting to 0000000001010190 )

Step 3 : powerpc64-fsl-linux-objcopy app.o -O binary app.bin.

Help me to sort out this problem ASAP .

Tags (1)
0 Kudos
Reply
1 Reply

1,484 Views
Pavel
NXP Employee
NXP Employee

Look at documentation for u-boot standalone application:

http://www.denx.de/wiki/view/DULG/UBootStandalone

 

See also "Standalone HOWTO:" in u-boot Readme file:http://git.denx.de/?p=u-boot.git;a=blob_plain;f=README;hb=HEAD
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply