PO4080ComExpress RCW file needed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PO4080ComExpress RCW file needed.

ソリューションへジャンプ
3,407件の閲覧回数
sumanthmushiger
Contributor III

Can any one give me the right/correct RCW binary / .cmm flash file for COMX-P4080 board ?

 

Or just tell me how can I flash the correct RCW for it ?

 

Here is the U-boot error I am getting.

I have attached the screenshot of it.

Please have a look at it. and also the RCW configuration that I used is attached.

 

10270_10270.pngpastedImage_1.png

Original Attachment has been moved to: flash_cfi.cmm.zip

Original Attachment has been moved to: Uboot.cmm.zip

Original Attachment has been moved to: demo_set_rcw_rev2.cmm.zip

タグ(2)
0 件の賞賛
返信
1 解決策
3,138件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

P4080COME-DS is produced by Emerson, you could get the latest Linux BSP and images from http://www.emersonnetworkpowerembeddedcomputing.com/, I found a document which should be useful for you, please refer to http://www.emersonnetworkpower.com/documents/en-us/products/embeddedcomputing/documents/documentatio....


If there is valid u-boot on another bank, please swith to that bank, and flash RCW to the altbank at the current bank.


If you have CodeWarrior TAP(USB TAP), you could use CodeWarrior to program RCW to flash, please refer to AN4267.pdf from Freescale Website.

CodeWarrior 10.3 provides support for P4080COME, if there isn't valid RCW on your target, you could use CodeWarrior JTAG configuration file in "CW_PA_v10.3.3\PA\PA_Support\Initialization_Files\jtag_chains" to connect to CodeWarrior, please refer to the section "Setting Up a Remote System to Use a JTAG Configuration File" in CW_PA_v10.3.3\PA\Help\PDF\Targeting_PA_Processors.pdf.



元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,139件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

P4080COME-DS is produced by Emerson, you could get the latest Linux BSP and images from http://www.emersonnetworkpowerembeddedcomputing.com/, I found a document which should be useful for you, please refer to http://www.emersonnetworkpower.com/documents/en-us/products/embeddedcomputing/documents/documentatio....


If there is valid u-boot on another bank, please swith to that bank, and flash RCW to the altbank at the current bank.


If you have CodeWarrior TAP(USB TAP), you could use CodeWarrior to program RCW to flash, please refer to AN4267.pdf from Freescale Website.

CodeWarrior 10.3 provides support for P4080COME, if there isn't valid RCW on your target, you could use CodeWarrior JTAG configuration file in "CW_PA_v10.3.3\PA\PA_Support\Initialization_Files\jtag_chains" to connect to CodeWarrior, please refer to the section "Setting Up a Remote System to Use a JTAG Configuration File" in CW_PA_v10.3.3\PA\Help\PDF\Targeting_PA_Processors.pdf.



0 件の賞賛
返信
3,138件の閲覧回数
sumanthmushiger
Contributor III

Thank you yipingwang. You reply was most helpful to me. And its very precise piece of information.

0 件の賞賛
返信