PCIe gen 2 detection issue with T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe gen 2 detection issue with T2080

2,268 Views
duraiselvi_dura
Contributor I

Hi,
I am working with T2080NXE8P1B  device  and i am facing PCIe Gen 2 detection issue with that device I need some help to solve the PCIe Gen 2 detection issue.(i.e) what may be possible reason for that?

Thanks in advance

0 Kudos
Reply
5 Replies

2,131 Views
duraiselvi_dura
Contributor I

Thank you for replay.

We configured PCI e gen2 x4 but its downgraded into gen1 x4 while booting.What could be reason for that? and Is that any options for changing de-emphasis level ? If possible kindly provide settings to change de-emphasis.level.

0 Kudos
Reply

2,131 Views
ufedor
NXP Employee
NXP Employee

The PCIe operation mode is negotiated with EP device.

You wrote:

> We configured PCI e gen2 x4

What exactly you have done?

0 Kudos
Reply

2,131 Views
duraiselvi_dura
Contributor I

Sorry for inconvenience caused.

We configured  EP PCIe as gen 1 x4 PCIe link was detected in T2080.If same  EP PCIe is configure as gen 2x4 means PCIe link was not detected. What could be the reason for not detection?

0 Kudos
Reply

2,131 Views
ufedor
NXP Employee
NXP Employee

There could be many reasons:

1) incorrect EP x4 Gen2 configuring

2) incorrect T2080 PCIe configuring in RCW

3) signal integrity issue affecting Gen2 operation.

Please provide processor connection schematics as searchable PDF and RCW binary image for inspection.

0 Kudos
Reply

2,131 Views
ufedor
NXP Employee
NXP Employee

> PCIe Gen 2 detection issue

What exactly does it mean?

0 Kudos
Reply