P5020 SATA extremely slow throughput

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P5020 SATA extremely slow throughput

2,258 Views
thomasesser
Contributor I

We are not able to achieve throughput in MBs using P5020 SATA

controller. The Kernel version is 3.0.6 i.e. DPAA v1.1 and sata

driver is fsl_sata.c.

Following is the u-boot output which shows board configurations:

U-Boot 2011.09 (Jan 16 2013 - 17:05:32)

CPU0:  P5020E, Version: 1.0, (0x82280010)

Core:  E5500, Version: 1.0, (0x80240010)

Clock Configuration:

       CPU0:1800 MHz, CPU1:1800 MHz,

       CCB:800  MHz,

       DDR:500  MHz (1000 MT/s data rate) (Asynchronous), LBC:100  MHz

       FMAN1: 400 MHz

       PME:   400 MHz

L1:    D-cache 32 kB enabled

       I-cache 32 kB enabled

Board: NAMC_P5020

Reset Configuration Word (RCW):

       00000000: 10540000 00000000 24240000 00000000

       00000010: 54402a00 c0002000 fe800000 01000000

       00000020: 00000000 00000000 00000000 00070000

       00000030: 00000000 00000000 00000000 00000000

I2C:   ready

SPI:   ready

DRAM:  Initializing....    DDR: 2 GiB (DDR3, 64-bit, CL=9, ECC off)

Flash: 128 MiB

L2:    512 KB enabled

Corenet Platform Cache: 2048 KB enabled

Bank1: PCIE1 PCIE1 PCIE1 PCIE1 PCIE2 PCIE2 PCIE2 PCIE2 NA NA

Bank2: XAUI_FM1 XAUI_FM1 XAUI_FM1 XAUI_FM1

Bank3: NA NA SATA1 SATA2

SRIO1: disabled

SRIO2: disabled

NAND:  1024 MiB

EEPROM: Read failed.

PCIe1: Root Complex, no link, regs @ 0xe0200000

PCIe1: Bus 00 - 00

PCIe2: Root Complex, no link, regs @ 0xe0201000

PCIe2: Bus 01 - 01

PCIe3: disabled

In:    serial

Out:   serial

Err:   serial

RapidIO: HOST device id 0x00000000, vendor id 0x00000000

RapidIO: PHY type: parallel

RapidIO: Port1 is trained successfully. ESCSR = 0x00000000

RapidIO: PHY type: parallel

RapidIO: Port2 is trained successfully. ESCSR = 0x00000000

magic number doesn't match. read 0xffff, must be 0xa570

BInfo: invalid

Net:   Fman1: Uploading microcode version 92.8.0

FM1@DTSEC4 connected to Broadcom BCM5461S

PHY reset timed out

FM1@DTSEC5 connected to Generic PHY

FM1@TGEC1 connected to Generic 10G PHY

FM1@DTSEC4, FM1@DTSEC5, FM1@TGEC1

Hit any key to stop autoboot:  5

Following is the Kernel logs of SATA along with HardDisk info:

fsl-sata e0220000.sata: Sata FSL Platform/CSB Driver init

scsi0 : sata_fsl

ata1: SATA max UDMA/133 irq 68

fsl-sata e0221000.sata: Sata FSL Platform/CSB Driver init

scsi1 : sata_fsl

ata2: SATA max UDMA/133 irq 69

ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata2.00: ATA-8: WDC WD5000BPVT-60HXZT3, 01.01A01, max UDMA/133

ata2.00: 976773168 sectors, multi 0: LBA48 NCQ (depth 0/32)

ata2.00: configured for UDMA/133

ata1: No Device OR PHYRDY change,Hstatus = 0xa0000000

ata1: SATA link down (SStatus 0 SControl 300)

scsi 1:0:0:0: Direct-Access     ATA      WDC WD5000BPVT-6 01.0 PQ: 0 ANSI: 5

sd 1:0:0:0: [sda] 976773168 512-byte logical blocks: (500 GB/465 GiB)

sd 1:0:0:0: Attached scsi generic sg0 type 0

sd 1:0:0:0: [sda] 4096-byte physical blocks

sd 1:0:0:0: [sda] Write Protect is off

sd 1:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't

support DPO or FUA

sda: sda1

sd 1:0:0:0: [sda] Attached SCSI disk

Following is the throughput test result:

namc-p4080:~# hdparm -t /dev/sda

/dev/sda:

Timing buffered disk reads:    2 MB in  3.31 seconds = 619.38 kB/sec

namc-p4080:~# hdparm -Tt /dev/sda

/dev/sda:

Timing cached reads:     2 MB in  3.02 seconds = 677.99 kB/sec

Timing buffered disk reads:    2 MB in  3.03 seconds = 676.78 kB/sec

Following is the driver status register:

SError(0x221104) => 0x00200900

LinkStatus1(0x221158) => 0xff000000

Any hint in getting the maximum throughput on reading/writing the SATA

disk will be highly appreciated.

Thanks and regards

Thomas

0 Kudos
Reply
3 Replies

1,896 Views
lunminliang
NXP Employee
NXP Employee

Please see technical support comment:

There is a patch to change TransCfg [RX_WATER_MARK ] at runtime, it can help performance, link is:

http://linux.freescale.net/patchwork/patch/21902/

Below is an example on p3041:

p3041ds login: root

root@p3041ds:~# uname -a

Linux p3041ds 3.8.10-rt6-00980-g67b6708 #2 SMP PREEMPT RT Tue May 21 19:26:17 CST 2013 ppc GNU/Linux root@p3041ds:~# find /sys/ -name rx_watermark /sys/devices/ffe000000.soc/ffe221000.sata/rx_watermark

/sys/devices/ffe000000.soc/ffe220000.sata/rx_watermark

root@p3041ds:~# cat /proc/interrupts | grep sata

68:          0          0          0         49 OpenPIC   Level     fsl-sata

69:          0          0          0          0 OpenPIC   Level     fsl-sata

root@p3041ds:~# cat /sys/devices/ffe000000.soc/ffe220000.sata/rx_watermark

16

root@p3041ds:~# hdparm -t /dev/sda

/dev/sda:

Timing buffered disk reads:  547 MB in 3.00 seconds = 186402 kB/s root@p3041ds:~# echo 18 > /sys/devices/ffe000000.soc/ffe220000.sata/rx_watermark

root@p3041ds:~# cat /sys/devices/ffe000000.soc/ffe220000.sata/rx_watermark

18

root@p3041ds:~# hdparm -t /dev/sda

/dev/sda:

Timing buffered disk reads:  600 MB in 3.00 seconds = 204785 kB/s root@p3041ds:~#


0 Kudos
Reply

1,896 Views
adeel
Contributor III

Hi Lumin,

Thanks for your answer. This problem is solved now. It was due to older revision of Silicon we were using.

Adeel

0 Kudos
Reply

1,896 Views
lunminliang
NXP Employee
NXP Employee

My pleasure, and thanks for sharing.

0 Kudos
Reply