P4080 internal loopback test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 internal loopback test

1,494 Views
ali_baspinar_el
Contributor I

Hey, i see a problem sometimes which is "couldn't get PHY for P4080DS_MDIO0 addr0 failed to connect" error. and ethernet not working at all. is it logical to make loopback test in processor and how?

0 Kudos
Reply
1 Reply

1,446 Views
Pavel
NXP Employee
NXP Employee

Ethernet PHY supports loopback mode. For example see the VSC8244 Data Sheet:

http://ww1.microchip.com/downloads/en/DeviceDoc/VMDS-10108.pdf

 

The P4080 SERDES does not support loopback mode.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply