P4080 WatchDog Timer - Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 WatchDog Timer - Interrupt

Jump to solution
2,819 Views
jameshorton
Contributor II

I'm doing some BSP work trying to get an interrupt to fire using hte Time Base Registers (upper/lower), Timer Control Register, Machine Status Register and either the HID0 or CTBENU/CTBSELU registers.

I see the TB is actively incrementing so it must be getting clocked.    I've written 0x0002_9000 to the MSR and tried two values (0x2804_0000, 0x3804_0000) in the TCR.   I never see the TSR change.  What else am I missing?  I haven't attached an interrupt handler yet but from what I'm seeing, I don't think it would be called yet.

1 Solution
2,539 Views
scottwood
NXP Employee
NXP Employee

You've selected bit 8 of the timebase for the watchdog to trigger.  With a timebase of 100 MHz (it's usually slower than that), you'd see bit 8 of the timebase flip after around 11.4 years.  Remember that the bits are numbered starting from the most significant bit.

View solution in original post

2 Replies
2,540 Views
scottwood
NXP Employee
NXP Employee

You've selected bit 8 of the timebase for the watchdog to trigger.  With a timebase of 100 MHz (it's usually slower than that), you'd see bit 8 of the timebase flip after around 11.4 years.  Remember that the bits are numbered starting from the most significant bit.

2,539 Views
jameshorton
Contributor II

That was the problem, I was counting the bits from the LSB. Thanks!

0 Kudos
Reply