P4080 SEC 4.0 Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P4080 SEC 4.0 Issue

2,102 Views
kuizhou
Contributor I

Hi there,

 

I met a P4080 SEC 4.0 issue which made me very confused. I'd be very appretiated if anyone could help.

 

The SEC 4.0 driver I used was downloaded from the Freescale web site and I just added some interface files in the attached "sec_interface.c" file to fit driver into our firmware. Files in the driver are not touched. The operationg system is vxWorks 6.8.

 

My usage of SEC 4.0 is very simple:-

    - Enqueue a request to SEC job queue to do Kasumi ciphering

    - Wait until the operation is done, then dequeue the ciphering result.

 

The above steps are implemented in one function called "kasumi_f8" which is in the attached "sec_interface.c" file. This function could be called by two simultaneously running tasks on two different CPU cores very frequently. Sometimes, the ciphering operation is never done and kasumi_f8 will enter dead loop intermittently. After some investigation, it turns out that the ISTAR of the job queue indicates that the JRE bit is set and ERR_TYPE is 0b1000 which means "Removed too many jobs".

 

Then I wrote a function below to check the error and try to do the recover. This function is called at the beginning of "kasumi_f8", and count the times of recovering. It seems that this function recovers the SEC several times successfully, and I never met the issue after running the test for more than 24 hours.

 

However, I could not understand what caused the SEC error. Does anyone encounter the same issue?

 

Regards,

Zhou Kui

 

#define ISTAR_JRE_BITMAP  0x2
#define ISTAR_HALT_BITMAP 0xC

t_Error SEC_JQ_Check_Recover(t_Handle h_SecJq)
   {
   uint32_t orsfr_val;
   t_SecJq* p_SecJq = (t_SecJq*)h_SecJq;

   SANITY_CHECK_EXIT(p_SecJq,E_INVALID_HANDLE);
   SANITY_CHECK_EXIT(p_SecJq->p_DriverParam==NULL,E_INVALID_STATE);

   if (GET_UINT32(p_SecJq->p_MemMap->jq.istar) & ISTAR_JRE_BITMAP)
      {
      /* JRE is set, Job Ring Error. Flush the Job Queue */
      WRITE_UINT32(p_SecJq->p_MemMap->jq.cmdr,1);

      /* Check if the Flush is completed */
      while ((GET_UINT32(p_SecJq->p_MemMap->jq.istar) & ISTAR_HALT_BITMAP)
             == 0x4)
         {
         /* Not completed, need to empty the job queue to keep the flush
          * running until it completes. */
         orsfr_val = GET_UINT32(p_SecJq->p_MemMap->jq.orsfr);
         if (orsfr_val != 0)
            WRITE_UINT32(p_SecJq->p_MemMap->jq.orjrr, orsfr_val);
         }

      /* Check if the Flush is completed again */
      if ((GET_UINT32(p_SecJq->p_MemMap->jq.istar) & ISTAR_HALT_BITMAP)
          != 0x8)
         /* Fatal error, we don't know what to do */
         {
         return E_JRE_NOT_RECOVERED;
         }
     
      /* Empty the job queue if there is any completed job left */
      orsfr_val = GET_UINT32(p_SecJq->p_MemMap->jq.orsfr);
      if (orsfr_val != 0)
         WRITE_UINT32(p_SecJq->p_MemMap->jq.orjrr, orsfr_val);
     
      /* Resume the job queue, and clear the error bits */
      WRITE_UINT32(p_SecJq->p_MemMap->jq.istar, 0xa);
      return E_JRE_RECOVERED;
      }
   else
      return E_OK;
   }

0 Kudos
Reply
1 Reply

1,773 Views
buckeyermc
Contributor I

kuizhou wrote:

Hi there,

 

 

 

The SEC 4.0 driver I used was downloaded from the Freescale web site . The operationg system is vxWorks 6.8.

 

 


Hello Kuizhou.

 

I'm afraid I can't offer any insight yet into your posted question as I'm just beginning my use of SEC 4.0 in a P4080.

I'd like to ask where did you obtain the SEC 4.0 driver you mentioned in your original post?  I have the Freescale_SDK but I think the driver you reference isn't in the SDK I'm trying to use.

 

If possible, can you please supply a reference link or file name of the SEC 4.0 driver that you downloaded.

 

Thanks for any assistance you can supply.

 

Regards,

    Rick.

0 Kudos
Reply