P3041DS bitbake build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P3041DS bitbake build error

1,623 Views
pete1
Contributor I

I have questions regarding the Yocto System Builder for the P3041DS.  Which forum should I post the messge to?

 

----

 

When I tried to build the ‘full’ image ($bitbake fsl-image-full) , I got the following error:

 

*** error: gettext infrastructure mismatch: using a Makefile.in.in from gettext version 0.17 but the autoconf macros are from gettext version 0.18

 

The full log is attached.  Any idea?

0 Kudos
Reply
0 Replies