P2020 processor kernel version

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 processor kernel version

2,884件の閲覧回数
rajendra_denduk
Contributor I

Hi,

Can someone comment on whether we can use upstream linux kernel (linux-4.14.y) on a  P2020 processor based board. Do we need the special drivers/bsp changes provided by freescale sdk. Last official release for QorIQ processors seems to be  on "fsl-sdk-v2.0-1701" which is linux-4.1 based.

Will I be missing anything if I am not using the NXP provided linux kernel for the P2020 processor based board?

Thanks.

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,776件の閲覧回数
jhering_ruegen
Contributor II

Hi all,

we use for our P2020 device (based on TQMP2020)

qoriq-components/linux - Linux Tree for QorIQ support 

NXP LSDK 20.04-V4.19 build via BuildRoot (Buildroot - Making Embedded Linux Easy )

the latest LT-Kernel  

NXP LSDK 20.04-V5.4 run always, but not complete tested yet.

Greetings from island Rügen

Jörg 

0 件の賞賛
返信

2,776件の閲覧回数
bpe
NXP Employee
NXP Employee

Consider using our Yocto-based SDK. It offers fresher kernels, including 4.14. and does support your processor:

qoriq-components/yocto-sdk - Repo manifest for QorIQ Yocto SDK 


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信