P2020 boot failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2020 boot failed

1,056件の閲覧回数
quray
Contributor I

I have a custom board and  burn uboot to nor flash successfully. Sometimes it can bring up and we can see the debug message . But most of time, P2020 boot failed and we can't see any debug message. The current DDR clock rate is 800MHz, the core clock rate is 400MHz. is there something wrong with the POR?

0 件の賞賛
返信
0 返答(返信)