P1022 System Version Register shows wrong value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1022 System Version Register shows wrong value

ソリューションへジャンプ
2,497件の閲覧回数
weiqing
Contributor II

Hi all,

We are using P1022 on our board, the model I find from the surface of the processor is:

P1022NXN2LFB

1066/667 MHZ

QQUU1529

MALAYSIA

1M79W    CXFCQAQ

However, U-Boot recognize only one core instead of two. And the System Version Register indicates that it is a P1013 processor, instead of P1022.

     U-boot=> md 0xff7e00a0 2

     ff7e00a0: 80211151 80e70011                      .!.Q....

From the P1022RM chapter 26.4.21, it says:

System version numbers for the chip system logic
0x80EE_0011 P1022 with security, dual core
0x80E6_0011 P1022 without security, dual core
0x80EF_0011 P1013 with security, single core
0x80E7_0011 P1013 without security, single core

Can someone explain me what may happens here? The value of SVR is read-only and is hard coded by Freescale, right?

Thanks for any advise,

weiqing

0 件の賞賛
返信
1 解決策
2,361件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Check TEST_SEL pin.  This pin must be pulled up. I may suppose it is pulled down on your board.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,361件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Check TEST_SEL pin.  This pin must be pulled up. I may suppose it is pulled down on your board.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,361件の閲覧回数
linzhou
Contributor II

Hi,

this pin is pulled up, do you have any other suggestion?

0 件の賞賛
返信