P1022 Power sequencing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P1022 Power sequencing

1,232 Views
zeevg
Contributor I

Hi,

The P1022 Power sequencing is (from DS):


1. VDDC, VDD, AVDD_PLAT, AVDD_DDR, LVDD2, OVDD2, AVDD_CORE0, AVDD_CORE1, BVDD, LVDD, OVDD,
SVDD, SVDD2, XVDD, XVDD2, SDAVDD, SDAVDD2


2. GVDD

What is the recommended delay between stage 1 to stage 2?

Pls. advise

Zeev Gerber

Tags (1)
0 Kudos
Reply
1 Reply

1,148 Views
alexander_yakov
NXP Employee
NXP Employee

There is no recommended delay between these voltages, the only maximum time is specified - all voltages must reach their values within 50 ms.

Minimum time between voltages from first line and voltage from second line - is not specified. The only requirement is - all voltages from first line must reach at least 90% from their values before voltage from second line reach 10%.

Also please note - this specific requirement is only in order to guarantee MCKE low during power-up. If there is no requirement for MCKE in your design, than specific sequencing for GVDD is not required.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply