P1010 can not boot from spi nor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P1010 can not boot from spi nor

887 次查看
袁增兴
Contributor I

Our project use p1010 + 2*H5TQ2G63GFR-RDC(DDR3 512MB) + 16M spi Nor,boot from spi nor.

It can not bootup,we can catch some spi clock,but just few spi clock.

It  does not issue a hardware reset request of the SoC by setting RSTCR[HRESET_REQ],so the eSPI loader code

find the  BOOT signature.

Why the eSPI loader code do not copy the user code?

Is the spihead.cfg right?
 

Original Attachment has been moved to: u-boot.spi.zip

Original Attachment has been moved to: spihead.cfg.zip

0 项奖励
回复
1 回复

749 次查看
ufedor
NXP Employee
NXP Employee

Are you avare that "u-boot.spi" already contains the header code?

I.e. only this one image has to be written to the SPI Flash?

0 项奖励
回复