Mount

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mount

1,161件の閲覧回数
tonymoseby
Contributor II

Hi, I have a new TWR-ls1021a  board.I can see there is a 1Giga nor flash on it. As such I would like to mount / into the norflash.(in order to keep my changes).In the preloaded system / is mount /dev/ram (I can see it in bootargs).Which device should I use to mount / into the nor flash? /dev/? Thanks

0 件の賞賛
返信
1 返信

1,129件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers Linux SDK for the TWR-LS1021board.

Look at documentation for this SDK on the following page:

http://www.nxp.com/products/software-and-tools/run-time-software/linux-sdk/linux-sdk-for-qoriq-proce...

 

See the Section 4.4.4.6 of the QorIQ SDK 2.0-1701 Documentation:

http://www.nxp.com/assets/documents/data/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

This Section provides information about NOR Flash usage on the TWR-LS1021a board.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信