MPC8347 CPU Local Bus Timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8347 CPU Local Bus Timing

1,489 Views
sharper
Contributor III

With the DLL in bypass mode and with OR[EAD] set to 0, LALE should be asserted for one bus clock cycle only.

What is the hold time of the LALE signal from the falling edge of LCLK?

Tags (2)
0 Kudos
Reply
1 Reply

1,302 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

It is not specified as for LALE as for LAD in the DLL bypass mode. Only LAD hold time from the falling edge of LALE is specified in this mode. It is supposed that address is latched on LALE transition while LCLK is irrelevant in this case.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply