MPC5643L - Download code with changes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5643L - Download code with changes

1,880件の閲覧回数
aratzrodriguezs
Contributor II

Hello,

I'm doing a master final project using MPC5643L and CodeWarrior for MPC55xx, MPC56xx 2.8.

One of the objectives of the project is to download code via serial communications (UART/CAN) while the program is running just with changes made from the version that is running. It would appreciate any ideas for doing this.

Thanks,

Aratz

0 件の賞賛
返信
2 返答(返信)

1,688件の閲覧回数
sarathchandra
Contributor III

Hi Aratz,

           Make your query little clear.

           Does you are expecting to run your code at u-boot ??

Regards,

Sarath

0 件の賞賛
返信

1,688件の閲覧回数
aratzrodriguezs
Contributor II

Hello,

I'm using a program that compiles from languages used in standard IEC 61131-3 to C.

So the idea is to have any application running on the platform and when I make a change in the program that uses 61131-3 standard, just send information regarding this program via CAN/UART.

Regards,

Aratz

0 件の賞賛
返信