MPC5643L - Download code with changes

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5643L - Download code with changes

1,898 次查看
aratzrodriguezs
Contributor II

Hello,

I'm doing a master final project using MPC5643L and CodeWarrior for MPC55xx, MPC56xx 2.8.

One of the objectives of the project is to download code via serial communications (UART/CAN) while the program is running just with changes made from the version that is running. It would appreciate any ideas for doing this.

Thanks,

Aratz

0 项奖励
回复
2 回复数

1,706 次查看
sarathchandra
Contributor III

Hi Aratz,

           Make your query little clear.

           Does you are expecting to run your code at u-boot ??

Regards,

Sarath

0 项奖励
回复

1,706 次查看
aratzrodriguezs
Contributor II

Hello,

I'm using a program that compiles from languages used in standard IEC 61131-3 to C.

So the idea is to have any application running on the platform and when I make a change in the program that uses 61131-3 standard, just send information regarding this program via CAN/UART.

Regards,

Aratz

0 项奖励
回复