Ls1020a lpuart with edma

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ls1020a lpuart with edma

1,105件の閲覧回数
ser_fr
Contributor I

Hello, can you help me to configure lpuart using edma transfer on ls1020a custom  board? And where l can find an example of using lpuart in linux application?

タグ(1)
0 件の賞賛
返信
1 返信

1,037件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Section 7.10.1 from SDK 2.0-1703 documentation about LPUART using:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信