LX2160A PRBS Under Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160A PRBS Under Linux

2,351 Views
HW_Team
Contributor I

Hi

We have used the CodeWarrior TAP for testing 10G-KR links however this doesn't allow for operation under Linux and ideally we would like to generate PRBS11 and PRBS31 codes under Linux and use these to exercise our partner device for bit error rate testing.

Would you please advise if there is a method for generating PRBS codes under Linux for a 10G-KR SERDES.

Thanks

Malcolm

0 Kudos
Reply
3 Replies

2,349 Views
ufedor
NXP Employee
NXP Employee

The only PRBS generation method supported by NXP is using CodeWarrior QCVS SerDes Tool.

0 Kudos
Reply

2,342 Views
HW_Team
Contributor I

Hi

Thank you for the feedback.

Is there a method to maintain the link under Linux whilst using the Codewarrior QCVS SerDes tool to modify the SerDes parameters? i.e. equalization settings.

Regards

Malcolm

0 Kudos
Reply

2,338 Views
ufedor
NXP Employee
NXP Employee

The CodeWarrior QCVS SerDes tool is intended to be used for standalone testing - i.e. there is no method to use it when a Linux link is maintaining.

0 Kudos
Reply