LX2160A PRBS Under Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160A PRBS Under Linux

2,398件の閲覧回数
HW_Team
Contributor I

Hi

We have used the CodeWarrior TAP for testing 10G-KR links however this doesn't allow for operation under Linux and ideally we would like to generate PRBS11 and PRBS31 codes under Linux and use these to exercise our partner device for bit error rate testing.

Would you please advise if there is a method for generating PRBS codes under Linux for a 10G-KR SERDES.

Thanks

Malcolm

0 件の賞賛
返信
3 返答(返信)

2,396件の閲覧回数
ufedor
NXP Employee
NXP Employee

The only PRBS generation method supported by NXP is using CodeWarrior QCVS SerDes Tool.

0 件の賞賛
返信

2,389件の閲覧回数
HW_Team
Contributor I

Hi

Thank you for the feedback.

Is there a method to maintain the link under Linux whilst using the Codewarrior QCVS SerDes tool to modify the SerDes parameters? i.e. equalization settings.

Regards

Malcolm

0 件の賞賛
返信

2,385件の閲覧回数
ufedor
NXP Employee
NXP Employee

The CodeWarrior QCVS SerDes tool is intended to be used for standalone testing - i.e. there is no method to use it when a Linux link is maintaining.

0 件の賞賛
返信