LS146A - Generic timer initialization

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS146A - Generic timer initialization

跳至解决方案
3,442 次查看
Chris_Avery
Contributor I

Attempting to initialize the system timer on a custom LS1046A board. The reference manual states the CNTFID0 (0x2b0_0020) register is undefined at reset and allows read/write access, but I can not write to the register. This is the first thing the software attempts to initialize at power-on. Does anyone know if there is some other interface that needs to be setup before this register can be written? 

0 项奖励
回复
1 解答
3,399 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following in ATF source code plat/nxp/soc-ls1046/soc.c

/*******************************************************************************
* Function to set the base counter frequency at
* the first entry of the Frequency Mode Table,
* at CNTFID0 (0x20 offset).
*
* Set the value of the pirmary core register cntfrq_el0.
******************************************************************************/
void set_base_freq_CNTFID0(void)
{
/*
* Below register specifies the base frequency of the system counter.
* As per NXP Board Manuals:
* The system counter always works with SYS_REF_CLK/4 frequency clock.
*
*/
unsigned int counter_base_frequency = get_sys_clk()/4;

/* Setting the frequency in the Frequency modes table.
*
* Note: The value for ls1046ardb board at this offset
* is not RW as stated. This offset have the
* fixed value of 100000400 Hz.
*
* The below code line has no effect.
* Keeping it for other platforms where it has effect.
*/
mmio_write_32(NXP_TIMER_ADDR + CNTFID_OFF, counter_base_frequency);

write_cntfrq_el0(counter_base_frequency);
}

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,420 次查看
yipingwang
NXP TechSupport
NXP TechSupport

my understanding is that you have to set the enable bit in the control register and make sure that the write access is in the EL3.

0 项奖励
回复
3,408 次查看
Chris_Avery
Contributor I

Thank you for answering me, but I had no luck with your suggestion. Assuming you meant the counter enable bit in CNTCR at 0x2b0_0000.

After verifying I was in EL3 I tried setting the Control register enable bit and it made no difference in the ability to write the CNTFID0 register. Nothing I do seems to change the contents of the CNTFID0 register.

I'm wondering if this is why I can't find an example writing to this register in uBOOT either.

If my initial assumption about the enable bit was wrong (i.e. I set the wrong enable bit), please let me know what enable bit you were referring to.

Thank you again.

标记 (1)
0 项奖励
回复
3,400 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following in ATF source code plat/nxp/soc-ls1046/soc.c

/*******************************************************************************
* Function to set the base counter frequency at
* the first entry of the Frequency Mode Table,
* at CNTFID0 (0x20 offset).
*
* Set the value of the pirmary core register cntfrq_el0.
******************************************************************************/
void set_base_freq_CNTFID0(void)
{
/*
* Below register specifies the base frequency of the system counter.
* As per NXP Board Manuals:
* The system counter always works with SYS_REF_CLK/4 frequency clock.
*
*/
unsigned int counter_base_frequency = get_sys_clk()/4;

/* Setting the frequency in the Frequency modes table.
*
* Note: The value for ls1046ardb board at this offset
* is not RW as stated. This offset have the
* fixed value of 100000400 Hz.
*
* The below code line has no effect.
* Keeping it for other platforms where it has effect.
*/
mmio_write_32(NXP_TIMER_ADDR + CNTFID_OFF, counter_base_frequency);

write_cntfrq_el0(counter_base_frequency);
}

0 项奖励
回复