LS1046A SPI/EMMC Pin Multiplex

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A SPI/EMMC Pin Multiplex

ソリューションへジャンプ
2,466件の閲覧回数
tian_shuliang
Contributor I

In LS1046A datasheet, SPI_PCS[0-3] and SDHC_DAT[4-7] are multiplexes。

If I want to use 8bit EMMC and SPI interface at the same time, how to design on hardware? Does the software have a corresponding driver?

pastedImage_1.png

0 件の賞賛
返信
1 解決策
2,351件の閲覧回数
r8070z
NXP Employee
NXP Employee

SPI shares signals with eSDHC in way that prevents using 8-bit eMMC and SPI at the same time. Functionality of SPI_PCS[0-3]/SDHC_DAT[4-7] pins is determined by the configuration word (RCW). The RCW is read from some nonvolatile memory on power-on reset (PORESET) only. The PORESET causes the chip to abort all current internal and external transactions and set all registers to their default values.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,352件の閲覧回数
r8070z
NXP Employee
NXP Employee

SPI shares signals with eSDHC in way that prevents using 8-bit eMMC and SPI at the same time. Functionality of SPI_PCS[0-3]/SDHC_DAT[4-7] pins is determined by the configuration word (RCW). The RCW is read from some nonvolatile memory on power-on reset (PORESET) only. The PORESET causes the chip to abort all current internal and external transactions and set all registers to their default values.

0 件の賞賛
返信