[LS1046A] Inquires regarding SDK and DDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LS1046A] Inquires regarding SDK and DDR

1,689件の閲覧回数
heesoo_ahn
Contributor I

To whom may it concern.

Hi, I'm HS.

I've been working on the project referenced LS1046ARDB and FRWY-LS1046A.

I found out FRWY-LS1046A populated DDR4 with ECC while LS1046ARDB used socket.

Q1. What's the difference in between FRWY-LS1046A and LS1046ARDB as to DDR4 for bring-up and control?

The system needs DDR4 8GB with ECC. Which one would be better? On board or socket?

Q2. I'm wondering if the SDK provide the source code as to DDR as well as other peripherals.

Q3. I'm wondering if the SDK is freeware.

I'm not sure if i can use these codes for business.

Do i need license contract for this?

Thank you.

0 件の賞賛
返信
2 返答(返信)

1,639件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello HeeSoo Ahn,

Q1 From controller perspective there is no difference between solder down DRAM and UDIMM or SoDIMM.

the difference is just for customer use case and requirements.

 

For 8GB with ECC both the DIMM and discrete DRAM are supported options. the choice is customer's decision on which one will fullfil thier use case and requirements.

Q2  SDK provides the source code as to DDR as well as other peripherals.

Q3 SDK is freeware.

Thanks,

Yiping

0 件の賞賛
返信

1,639件の閲覧回数
heesoo_ahn
Contributor I

Hello Yiping.

I found out that FRWYLS1046A populated DDR4 4GB.

I wanted to use DDR4 8GB and would really appreciate if you tell me which part i should change in source code regarding DDR4 in SDK.

Thank you!

0 件の賞賛
返信