[LS1046A][DPAA1] Kernel crashes after PCD distribution queue to TX FQID.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1046A][DPAA1] Kernel crashes after PCD distribution queue to TX FQID.

4,009 Views
alance
Contributor II

Hi

I set TX FQID on the PCD distribution queue to forward traffic bypass CPU. The fmc can execute the policy successfully. However, the kernel crashes after I send the packet for PCD to another TX FQID. Related info and configurations are attached. Any suggestions would be appreciated.

 

root@localhost:~# [  791.043545] Unable to handle kernel paging request at virtual address deadbeefdeadbfbf

[  791.051469] Mem abort info:

[  791.054263]   Exception class = DABT (current EL), IL = 32 bits

[  791.060176]   SET = 0, FnV = 0

[  791.063223]   EA = 0, S1PTW = 0

[  791.066354] Data abort info:

[  791.069228]   ISV = 0, ISS = 0x00000004

[  791.073060]   CM = 0, WnR = 0

[  791.076020] [deadbeefdeadbfbf] address between user and kernel address ranges

[  791.083152] Internal error: Oops: 96000004 [#1] PREEMPT SMP

[  791.083153] Modules linked in: xt_addrtype xt_conntrack crc32_ce lm90 ina2xx

[  791.083163] CPU: 1 PID: 728 Comm: irq/27-QMan por Not tainted 4.14.53-rt34 #3

[  791.083165] Hardware name: LS1046A COBRARDB Board (DT)

[  791.083166] task: ffff800972bec740 task.stack: ffff00000c758000

[  791.083176] PC is at _dpa_cleanup_tx_fd+0x50/0x348

[  791.083179] LR is at priv_tx_conf_default_dqrr+0x70/0x130

[  791.083180] pc : [<ffff0000088cc600>] lr : [<ffff0000088cb730>] pstate: 80000145

[  791.083181] sp : ffff00000c75bb20

[  791.083182] x29: ffff00000c75bb20 x28: 0000000000000003

[  791.083184] x27: 0000000000000000 x26: ffff8008cc88df40

[  791.083186] x25: ffff80097f776cc0 x24: ffff800971523098

[  791.083188] x23: ffff800971537980 x22: ffff000009255000

[  791.083190] x21: ffff80097f7770d0 x20: deadbeefdeadbeef

[  791.083191] x19: 000000094c88df40 x18: 0000000000003f30

[  791.083193] x17: 00004000927f54c0 x16: 0000400092687b80

[  791.083197] x15: 57de11ef307e56a4 x14: 0000000000000000

[  791.083199] x13: ffff80097f778368 x12: 0000000000000001

[  791.083200] x11: 0000000000000003 x10: 0000000000000a50

[  791.083202] x9 : ffff00000c75bd70 x8 : ffff800972bed1f0

[  791.083203] x7 : 0000000000000000 x6 : 0000000000000003

[  791.083205] x5 : 0000800976370000 x4 : 0000000000000000

[  791.083207] x3 : ffff0000088cb6c0 x2 : 00000008cc88df40

[  791.083208] x1 : 0000000080000000 x0 : ffff80097279bc10

[  791.083211] Process irq/27-QMan por (pid: 728, stack limit = 0xffff00000c758000)

[  791.083212] Call trace:

[  791.083214] Exception stack(0xffff00000c75b9e0 to 0xffff00000c75bb20)

[  791.083216] b9e0: ffff80097279bc10 0000000080000000 00000008cc88df40 ffff0000088cb6c0

[  791.083218] ba00: 0000000000000000 0000800976370000 0000000000000003 0000000000000000

[  791.083220] ba20: ffff800972bed1f0 ffff00000c75bd70 0000000000000a50 0000000000000003

[  791.083221] ba40: 0000000000000001 ffff80097f778368 0000000000000000 57de11ef307e56a4

[  791.083223] ba60: 0000400092687b80 00004000927f54c0 0000000000003f30 000000094c88df40

[  791.083224] ba80: deadbeefdeadbeef ffff80097f7770d0 ffff000009255000 ffff800971537980

[  791.083226] baa0: ffff800971523098 ffff80097f776cc0 ffff8008cc88df40 0000000000000000

[  791.083227] bac0: 0000000000000003 ffff00000c75bb20 ffff0000088cb730 ffff00000c75bb20

[  791.083229] bae0: ffff0000088cc600 0000000080000145 ffff800971537980 ffff800971bb7318

[  791.083230] bb00: ffffffffffffffff ffff80097f777090 ffff00000c75bb20 ffff0000088cc600

[  791.083233] [<ffff0000088cc600>] _dpa_cleanup_tx_fd+0x50/0x348

[  791.083235] [<ffff0000088cb730>] priv_tx_conf_default_dqrr+0x70/0x130

[  791.083240] [<ffff000008b39970>] qman_p_poll_dqrr+0x230/0x260

[  791.083242] [<ffff0000088cb320>] dpaa_eth_poll+0x20/0x58

[  791.083245] [<ffff000008bbc08c>] net_rx_action+0x18c/0x320

[  791.083248] [<ffff0000080ca3e4>] do_current_softirqs+0x1b4/0x268

[  791.083250] [<ffff0000080ca4ec>] __local_bh_enable+0x54/0x68

[  791.083253] [<ffff00000811bc3c>] irq_forced_thread_fn+0x64/0x90

[  791.083254] [<ffff00000811bf24>] irq_thread+0xfc/0x198

[  791.083257] [<ffff0000080e53cc>] kthread+0x12c/0x130

[  791.083260] [<ffff000008084d80>] ret_from_fork+0x10/0x18

[  791.083264] Code: 7102001f b251405a f9400b00 f9400354 (f9406a82)

[  791.376642] ---[ end trace 0000000000000002 ]---

[  791.376669] genirq: exiting task "irq/27-QMan por" (728) is an active IRQ thread (irq 27)

 

0 Kudos
Reply
1 Reply

3,989 Views
yipingwang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply