LS1046 RDB : "Qman ErrInt: Invalid Enqueue State"  error being displayed during packet reception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 RDB : "Qman ErrInt: Invalid Enqueue State"  error being displayed during packet reception

2,625 Views
veereshsajjan
NXP Employee
NXP Employee

Hi ,

I'm working on DNI custom LS1046A RDB boards.

And I have changed the custom dts changes to the latest ASK7.0.1.B1, build and flashed kernel image.

 

when I configure ip address on interface and try to ping from remote end, below error is being observed.

 

Qman ErrInt: DCP id 0
Qman ErrInt: ecir.fqid 0x10255
Qman ErrInt: Invalid Enqueue State
Qman ErrInt: DCP id 0
Qman ErrInt: ecir.fqid 0x10255
Qman ErrInt: Invalid Enqueue State
Qman ErrInt: DCP id 0
Qman ErrInt: ecir.fqid 0x10255
Qman ErrInt: Invalid Enqueue State.

 

The above observation is for eth0 interface but when I configured the IP on eth1 interface and perform ping, ping is successful without any errors 

 

I have attached the dts file for your reference, Please provide some inputs to resolve this issue quickly.

 

Thank you 

Original Attachment has been moved to: fsl-ls1046a-rdb.dts.zip

0 Kudos
Reply
1 Reply

2,332 Views
d-z-c
Contributor III

HI @veereshsajjan 

Do you have a good answer about this issue now? 

If yes,could you share it?

Best wishes.

Have a good day.
Tags (2)
0 Kudos
Reply