LS1043ARDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043ARDB

2,194件の閲覧回数
lingguan
Contributor II

Hi experts,

I have a question about using LS1043ARDB to achieve some applications.

How do write C/C++ program to control some GPIOs and ethernet port ?

Sincerely.

0 件の賞賛
返信
3 返答(返信)

2,015件の閲覧回数
Pavel
NXP Employee
NXP Employee

Yes, it is possible. Use CodeWarrior for Linux for your task.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,015件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior compiler:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

This CodeWarrior can be used for developing standalone application and Linux application. Evaluation version for CodeWarrior supports full functionality during 30 days.

 

The simplest way if Linux sysfs possibility is used for control GPIO or Ethernet.

See the following pages:

http://www.6by9.net/using-linux-sys-to-disable-ethernet-hardware-devices/

 

https://www.kernel.org/doc/Documentation/gpio/sysfs.txt

 

https://elinux.org/GPIO


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,015件の閲覧回数
lingguan
Contributor II

Thank you very much for your reply.

I don't have JTAG for CodeWarrior. Could I first write program in CodeWarrior, and then copy program to Linux environment for cross compile?

0 件の賞賛
返信