DMA_BIT_MASK for PowerPC Qoriq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA_BIT_MASK for PowerPC Qoriq

391 Views
amarnathsubrama
Contributor II

 We are trying to port custom pci based alsa driver on our custom board with Qoriq processor.

 when the driver is loaded,got below error, 

 [  120.014015] CTI_ALSA:  module init called, index=[1] 
 [  120.017797] CTI_ALSA:  device set 24bit DMA mask failed w/err=[0]

  The error occurs when i do dma_set_mask for 24bit

  /*
     if ((err = dma_set_mask(&pcidev->dev, DMA_BIT_MASK(24))) < 0) {
        printk(KERN_ERR CTI_PREFIX " device set 24bit DMA mask failed w/err=[%d]", err);
        err = -ENXIO;
        goto err_disable_dev;
        }

        if ((err = pci_set_consistent_dma_mask(pcidev,DMA_BIT_MASK(24)) < 0)) {
        printk(KERN_ERR CTI_PREFIX " device set 24bit consistent DMA mask failed w/err=[%d]", err);
        err = -ENXIO;
        goto err_disable_dev;
        }

  */

  The same driver is working fine with Intel processor.

  Let me know, if i need to do any change w.r.t Qoriq processor.

0 Kudos
1 Reply

326 Views
ufedor
NXP Employee
NXP Employee

Please consider that the PowerPC processor is big-endian.

Refer to the following application note:

https://www.nxp.com/docs/en/application-note/AN2285.pdf 

0 Kudos