LS1043ARDB RootFS on SD chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB RootFS on SD chip

5,145 Views
donberkowitz
Contributor II

I am trying to initialize an SD Chip using the instructions on Page 69 of SDK version 0.5 PDF which read:

#cp fsl-image-core-ls1043ardb_<release date>.rootfs.tar.gz temp/

#tar xvfz fsl-image-core-ls1043ardb_<release date>.rootfs.tar.gz

#rm fsl-image-core-ls1043ardb_<release date>.rootfs.tar.gz temp/

I have several questions:

1) I built the x11 image - it produces a file with an extension rootfs.ext2.gz but does not build a rootfs.tar.gz file.  The instructions suggest that the file needs to be uncompressed and un-tar'ed on the SD chip.  Is that correct?

2) The first instruction puts the fs on the SD chip, but don't the instructions need to cd to temp before un-tarring?

3) If these instructions are wrong, what are the correct instructions?

Thanks,

Don

0 Kudos
Reply
6 Replies

5,000 Views
Pavel
NXP Employee
NXP Employee

1) Use the rootfs.ext2.gz file instead of rootfs.tar.gz file.

2) Yes, instruction for change directory is needed.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,000 Views
donberkowitz
Contributor II

There was no screenshot attached. Can you please provide?

Thanks,

Don

0 Kudos
Reply

4,999 Views
Pavel
NXP Employee
NXP Employee

See attachment.
Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,999 Views
donberkowitz
Contributor II

I had asked several questions, but do not see any answers in the screenshot attached.

0 Kudos
Reply

4,999 Views
Pavel
NXP Employee
NXP Employee

Look at the following page:

https://community.freescale.com/message/613599?et=watches.email.thread#613599
Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,999 Views
donberkowitz
Contributor II

Thank you Pavel.

1) So the U-Boot loader can accept an ext2.gz file and boot load from it, yes?

2) Can U-Boot also accept an unzipped file as well?

3) Will it boot faster if the file is unzipped prior to storing on the SD chip?

I have numbered the questions in the hope that you will answer each one.

Thanks!

Don

0 Kudos
Reply