LS1043A net RGMII & PCIe bandwidth?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A net RGMII & PCIe bandwidth?

1,963 Views
mike_palmer
Contributor II

Custom LS1043A board w/2GB DDR3.

We have an M.2 WiFi card on a PCIe lane and 2 GbE RGMII ports.

Any one of them will do a Gb (RGMII ports yes, the WiFi card comes in at around 800Mbps) on its own using iPerf. If we add one more channel (i.e. if we're running RGMII1 and start iPerf on RGMII2) then both RGMII channels report roughly 460Mbps each.

If we add the WiFi then all three are shown ~300Mbps.

IOW, it seems like the total bandwidth is 1Gbps shared between these channels.

Is this expected? Is there a choke point in the architecture that causes this?

0 Kudos
Reply
3 Replies

1,949 Views
mike_palmer
Contributor II

Thanks @yipingwang . At first we used the defaults and then tried:

iperf3 -c <server-ip-here> -B <client-ip-here> -t 0 -p 5201 --length 9018

and

iperf3 -c <server-ip-here> -B <client-ip-here> -t 0 -p 5201 --set-mss 1460

 

with neither providing any improvement.

May I ask what parameters or command-line arguments were used to correct the issue on the RDB?

 

 

0 Kudos
Reply

1,938 Views
yipingwang
NXP TechSupport
NXP TechSupport

1.  Please run the following iperf commands on the server and client sides.

 

Sever: iperf  -s

 

Client:

iperf -c 10.10.10.2 -P 10 -t 30

 

 2. When doing iperf performance test, please compile Linux Kernel with CONFIG_NETFILTER and CONFIG_CPU_FREQ disabled.

 

3. Please run FMC tool.

$ cd /etc/fmc/config/private/ls1043ardb/RR_FQPP_1455

$ fmc -c config.xml -p policy_ipv4.xml -a

0 Kudos
Reply

1,952 Views
yipingwang
NXP TechSupport
NXP TechSupport

What is the frame size which you are using in your testing?

If you are using small frame size, this test result is similar as LS1043ARDB provided by the testing team.

0 Kudos
Reply