LS1043A - Secure boot from QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A - Secure boot from QSPI

2,677件の閲覧回数
jeremy_sauget
Contributor I

I am using an LS1043A based board and I am trying to use secure booting from QPSI. As I am facing some issues, I did some research but I did not find any example or previous post saying it as already been done successfully.

Does anyone already did it ?

Thanks in advance for your help.

0 件の賞賛
返信
3 返答(返信)

2,549件の閲覧回数
ufedor
NXP Employee
NXP Employee

Secure boot from QSPI is supported for the LS1043A.

It is possible to use LS1046ARDB QSPI secure boot as example.

0 件の賞賛
返信

2,550件の閲覧回数
jeremy_sauget
Contributor I

Hi ufedor,

Thanks for your answer. I already had a look on LS1046A example but I was interested in having a ready to go example to test on my LS1043A board to see if I can make it work before applying it to my specific case.

0 件の賞賛
返信

2,550件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no such example for the LS1043A because the LS1043ARDB lacks a SPI flash connected to the QSPI interface.

0 件の賞賛
返信