LS1043A IFC clock generation during power-on-reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A IFC clock generation during power-on-reset

Jump to solution
1,321 Views
michael_machesk
Contributor I

Hi,

Question on the generation of clock outputs by the LS1043A processor during the power-on-reset sequence.  While PORESET_B is being held asserted to the LS1043A will the processor generate a clock output on IFC_CLK?  Or does PORESET_B need to be deasserted first for the LS1043A to start generating a clock output on IFC_CLK?

Thanks,

Mike

0 Kudos
Reply
1 Solution
1,262 Views
ufedor
NXP Employee
NXP Employee

> While PORESET_B is being held asserted to the LS1043A will the processor generate a clock output on IFC_CLK?

No.

> Or does PORESET_B need to be deasserted first for the LS1043A to start generating a clock output on IFC_CLK?

Yes.

View solution in original post

0 Kudos
Reply
1 Reply
1,263 Views
ufedor
NXP Employee
NXP Employee

> While PORESET_B is being held asserted to the LS1043A will the processor generate a clock output on IFC_CLK?

No.

> Or does PORESET_B need to be deasserted first for the LS1043A to start generating a clock output on IFC_CLK?

Yes.

0 Kudos
Reply